AOUT#.VALUEU

Description

Gets or sets the user command value of the specified analog output when AOUT#.SOURCE = 0 (user).

Examples

Usage

When AOUT#.SOURCE = 0 (user) then the corresponding AOUT#.VALUEU is used to drive the AOUT#.VALUE .

Code

Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:

--> AOUT1.SOURCE 0 //user
--> AOUT1.VALUEU
0.000 V
--> AOUT1.VALUE
0.000 V
--> AOUT1.VALUEU 1
--> AOUT1.VALUE
1.000 V

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units V
Range 0 to 10
Default Value 5
Data Type Float
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.VALUEU

3800h

06h

Signed16

-

1000:1

Read/Write

Yes

AOUT2.VALUEU

3801h

06h

Signed16

-

1000:1

Read/Write

Yes